Hi, I have a legacy High Speed Digital Interface Board Version 4.4(ACTIVE) WAVEVSN-BRD-4.4 which I would like to keep using but not sure if it is any good for the newer or older 10-100 Msps ADS and DAC boards. There are several A/D and D/A boards listed on the TI product site which should be OK, but its not clear whether these are the only ones compatible. Also I could not find any info if the board released before WV4.4 can be interfaced to PC using WAVEVSN-BRD-4.4. Any comments or references to TI documentation or application notes would be appreciated.