This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS41B49 + TSW1400

Other Parts Discussed in Thread: ADS41B49, ADS4149, ADS58B18

Hi

We have a customer using the ADS41B49 and TSW1400. 

TSW1400 board connected to USB on computer and running 5V Wall port. Also connected directly to the ADS41B49 Eval board, which is being powered by an external 3.3V source (into the 3.3V and Ground jacks). Clock input to the ADS41B49 board (25MHz at +10dBm) into J19. Signal of interest (6MHz @ -40dBm) into J6 on the ADS41B49 board.

 Seeing phenomena where the noise floor randomly gets about 30 – 50dB higher, then jumps back down. It seems to happen at random intervals between 20 and 50 seconds apart..  See attached word document. 

2727.Problems with TI TSW1400 Board paired with ADS41B49 Eval Board.docx

Thanks for your help.

Regards,

John Wiemeyer