Hello,
I have a problem about my board "TSW1400".
I have installed the Pattern Generator "TSW1400" with "DAC 5681". However, I changed my computer to windows 7 system. I find that "DAC 5681" can not communicate with my computer. I searched the problem and find the answer with the following site:
http://e2e.ti.com/support/data_converters/high_speed_data_converters/f/68/t/102652.aspx
In the forum, they give the solution with the following site:
http://e2e.ti.com/support/data_converters/high_speed_data_converters/f/68/t/85288.aspx?PageIndex=2
In this question, they told a solution using "usb_ser.zip". Therefore, I tried to use "usb_ser.zip" to make my DAC board communicate with the computer. However, I make a mistake that when I serialize the USB, both the "TSW1400" and "DAC 5681" are connected to my computer. So after serialize the USB, I find that my "TSW1400" can not communicate with the computer. When the computer detect the connection of "TSW1400", the name of new device "TSW1400" become that of "DAC 5682". Now I can not use "TSW1400" neither...
Could you please tell me that if you have the solution to serialize the USB of "TSW1400"? Like in the "usb_ser.zip" in the http://e2e.ti.com/support/data_converters/high_speed_data_converters/f/68/t/85288.aspx?PageIndex=2
Thank you very much for your help.
Linning