Good afternoon,
I just bought the DAC5687EVM and it comes with an USB-SPI Adapter.
However, it looks like its driver just works with window XP. There is a driver for windows 7, or windows 7 compatible?
Or it is possible to convert it? As the technical support / updates for Windows XP are no longer available, it is not so good idea to continue based on windows xp...
It's that possible, or it is possible to use the original FTDI Drivers changing something?
Another point, later I will connect the DAC to a FPGA. So that, I would like to program the DAC directly throught the FPGA and not through USB in the Windows XP... Do you some files/documents/protocol that could help me with the programming? That would be great.
Thanks in advance.
Best regards,
Susana