Hello,
I am using the ADC12D1600RFRB for digitizing signal in continuous time interval of 10msec. For this purpose I use memory capture platform Xilinx ML-605, which has sufficient on-board memory to provide deep data capture. The boards are interconnected by the FMC connector
I have build the setup according to the instructions given in the file ML605_Setup_Guide_v8.docx ( being contained in the zipped package) available at the following link: http://e2e.ti.com/cfs-file.ashx/key/communityserver-discussions-components-files/68/8662.GHz_5F00_ADC_5F00_package.zip)
The documentation states that the WaveVision should be equipped with a modified firmware for the ADC evaluation board. The only firmware provided in the mentioned package is image file named adc10d1000_xc4vlx25_adc12d1600rfrb.bit.
I analyzed the sampled data and found a lot of incorrect readouts (distortions) in accumulated batch. Trying to find out about the reason for the problem, we noticed that the WaveVision indicates the ADC sampling rate of 1800MHz. Taking into account, that our ADC board is specified for 1600MHz rate, I suppose that the available image file is not compatible with our HW.
Can You provide the appropriate image file for the ADC12D1600RFRB board, for operating at 1600 MHz sampling speed?
Additionally, could you provide some detailed guidance or suggestions for successful activation of the setup described above.
Best regards,
Boris