I am using the ADC12J4000EVM together with the TSW14J56EVM. The SW I use is High Speed Data converter Pro 2.6, together with the ADC12J400EVM GUI version 1.3
The TSW has enough memory for 500M samples. I set up the sampling buffer size with the CAPTURE OPTION tab
Getting the samples out of the card takes very long time, significantly much longer than what would be justified by the USB interface. It seems that SW graphics and File system service are the problem. it can take more than 30 minutes to extract one buffer.
Questions
1. is the an alternative mechanism to read the sample buffer from the TSW14J56EVM? for instance, buy my own application?
2. what is the binary file format?
Boaz