I am using the ADC12J4000EVM together with the TSW14J56EVM. The SW I use is High Speed Data converter Pro 2.7, together with the ADC12J400EVM GUI version 1.3
I am testing the ADC12J4000 in a computerized set up where I change the settings and read the measured samples to files for various conditions and signals.
I am looking for a mechanism (non-manual) to change the ADC12J400 internal digital mixer (NCO frequency) from test to test. My prefered option would be to write NCO_FREQ values. Alternatively, if I can pre-program frequencies and only change the NCO preset selection value -- this would also save me time and effort.
Regards
Boaz