We drive the DAC5682 SPI bus from an FPGA 3.3V bank. We see the "1" SPI signal levels at around 3V before a 22 ohm series termination resistor, but after the termination resistor at the DAC5682 pin the "1" level is only at 1.8V.
The DAC5682 supply voltages as measured at the power pins are: Vdvdd = 1.8V, Viovdd=3.3V, Vavdd=3.3V
What could be the issue? Is the DAC5682 somehow clamping the levels at 1.8V?
Thank you,
Valentin