Hello,
We have a customer that has the AFE7070EVM hooked up to the TSW4100. They set up the AFE7070 for dual output clock mode so they followed the reccomendations of 1.4.2 in the User's Guide (Couple of changes to resistors).
http://www.ti.com/lit/ug/slou337/slou337.pdf
The eval system looks to be working correctly. Bits are toggling at the output CMOS header into the AFE7070 board. The AFE7070 is hooked pin 1 to 1 , 2 to 2 ,… and so on up to pin 34 of the AFE. Specs:
1) 120 MHz Wenzel oscillator hooked to the LO input of the AFE.
2) J12 (ext clk) is connected to a 65 MHz signal generator set to 7 dBm.
3) CLK IO sma is connected to cmos clk on the TSW using a short SMA.
On the output there only seems to be a 120 MHz LO signal. We are lookng for help on how to set up the GUI so that a QAM generator can be created. On the High speed Data Converter Pro v2.70 screen the correct(simulated) waveforms are displayed, and the send command seems to work. The device is set to: CMOS_AFE7070. The problem seems to be in the AFE software and control. What other information should I supply?
Thanks,
Eric