Hi,
I'm using the LM97600RB and I wish to automate the signal capture process based on a trigger so that the board keeps capturing data without having to initiate the capture from WaveVision. However, some of the functions such as the Sync Req have to be performed on WaveVision before we can acquire the data. Wouldn't it be possible to ensure that the FPGA does this on initialization rather than having us to perform this to ensure that the correct data is being captured ?