I have two ADC12J4000EVM boards and both boards behave the same way. There must be something basic I'm missing?
The usb is connected to a Win7 laptop with USB and the ADC12J400EVM GUI v1.3.
The FTDI is connected and I can program the clocks on the board, green lights, but the Temperature Sensor is red.
I can not read or write the Temp Sensor (read LM95233 produces FFs). This happens on two boards.
The board is not plugged into another board (straight out of the box). Any suggestions?
Thanks,
John