Hello, I am testing the ADC12J4000EVM eval board and need to compute the absolute power in dBm into the ADC. I have a measurement of power at the input to the board @ the RF input SMA connector. I assume there is some insertion loss and a matching network on the front end that attenuates the input before RF is provided to the ADC. Can anyone help translate power into the board to power into the ADC?