I have an ads42LB69 that I dc-couple through a differential amplifier. I see an exaggerated response when I apply a square wave, there is no ringing just 75mV of overshoot followed by a 2us decay. I don't have any distortion issues with sine wave input (good SFDR and SNR). I am able to probe the input to the ADC and do not see this amount of overshoot/decay. I have bypassed the amplifier and driven the ADC direct single ended (offset to VCM) and see the same response. I ran the same experiment on an ADS62P49 and do not see the problem.