Hi there.
I am having problems with the ADS823 converter. I used the recommended circuit shown in the Fig. 2. of the datasheet but I am only getting one bit conversion output. I mean, every out pin gives the same output voltage. When the input signal has more than 2,5 V the output is "1111111111", and when it is less than 2,5 V the output is "0000000000". I think the problem is related to the ByB and ByT PINs, cause I let both of them open. However, the datasheet does not give enough information about their mission, or I am not understanding it.
Could be my problem related to those pins? Should I bypass and connect them to ground? What is the function of those pins?
Thank you very much for your attention.
Óscar