ADS 5400 datasheet describes the behavior as Over Range (OVRA) flag occurs, which can indicate either below or above the full range input of ADC. The datasheet doesn't really say whether it will cap the data value to max or min when over range occur. Please advise if the device will automatically saturate to all 1's for max or 0's for min.
While the datasheet show an expected error a clock after over range flag to at most 25%, is there any indication whether the lower or upper bound was in violation?
As a follow-on question in relates to Reset and Clock, if we decided it is necessary to perform a reset to the system (ADC), and the reset line is driven in such a way that it is a multiple of 8x input clock pulse, aligned with the CLKINP/N (@ 300 Mhz) in single bus mode.
I was informed from testbench result that the clock remain free running during reset, but would like to understand further on the expected behavior of CLKCOUT.
We plan to periodically issue a reset every 1/3 of a second when performing FFT elsewhere on board.
Upon reset, will ADS5400 momentarily use the default divider from register setting and/or possibly introduce a slight distortion to the clock?
How much more alignment effort will the ADS5400 perform based on the incoming reset to the free running input clock to maintain a continuous free running divided by 2 clock? Will dramatic board temperature affect the reset point and cause a glitch during and immediately coming out of the 7-cycle latency?
Thanks much for any comment and feedback!