Hello,
DACCLKP/N input requirments are 0.5V common-mode and 800mV differential peak-to-peak, so I would like to know the reason of the decoupling capacitor of Figure 75 in the datasheet that removes the common-mode input voltage.
thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
The DACCLK input self-biases to the correct common mode voltage. The DC blocking caps allow the clock driver and the DACCLK input to bias to their respective common mode voltages. LVPECL has a much higher common mode voltage, closer to 2V.
Regards,
Matt Guibord
HI Matt
Can the SYSREF and the DACCLK Vcom be externally DC Biased to higher voltages? How high and how can Vcom safely be driven? Perhaps there is a more detailed equivalent circuit for this that includes the internal bias on these pins?
We have a case where we would like to DC couple the SYSREF and make the DACCLK coupling identical.
Figure 75 in the data sheet (AC coupled example) shows the receiver equivalent circuit as a floating 100 Ohm differential termination and Vcom specification is 0.5V typical but no min or max?
On the eval board where SYSREF appears to be DC coupled, Vcom looks more like upwards of 0.55V than 0.5V?
Like the eval board, to DC couple SYSREF, we would use a voltage divider, which also divides the signal amplitude.
How high can we safely go on Vcom so we can maximize the signal?
Thanks Dave
Dave Lewis93983 said:HI Matt
Can the SYSREF and the DACCLK Vcom be externally DC Biased to higher voltages? How high and how can Vcom safely be driven? Perhaps there is a more detailed equivalent circuit for this that includes the internal bias on these pins?
We have a case where we would like to DC couple the SYSREF and make the DACCLK coupling identical.
Figure 75 in the data sheet (AC coupled example) shows the receiver equivalent circuit as a floating 100 Ohm differential termination and Vcom specification is 0.5V typical but no min or max?
On the eval board where SYSREF appears to be DC coupled, Vcom looks more like upwards of 0.55V than 0.5V?
Like the eval board, to DC couple SYSREF, we would use a voltage divider, which also divides the signal amplitude.
How high can we safely go on Vcom so we can maximize the signal?
Thanks Dave
Hi,
I have the exact same issue ! How can the datasheet mention the LVPECL standard, if the internal common mode voltage of the SYSREF pins are 0.5V ?
Does it mean it is impossible to implement a LVPECL DC coupled communication for the SYSREF signal ? Because that's what i planned in my application, and I'm worrying about this datasheet's value atm ...
Thanks,
Alexis