Hello,
I have 4 pieces ADS5407 connected to an Altera FPGA. They seem to work well converting analog inputs.
Using the 3-pin SPI, I try to enable the test pattern mode.
Writing and reading to/from registers 3C and 3D works well, but register 3E reads back FFFF, no matter what I write.
Note that I can have the ADS5407s output all 0s, by writing 0x8000 to register 0x3C, but I can't make them toggle any pattern.
I do set HP1=0 (Addr 0x01, D01) before all this.
Is there something I'm missing here?
Thanks,
Mircea