The schematic for the DAC34H84EVM shows a 5th-order LPF at each output. Contained in this LPF are inductors and capacitors, as expected, but the caps are DNI and the inductors are 0-ohm resistors. For example, D1/D2 output has L27, L28, L29 and L30 shown as inductors, BOM has them as 0-ohm resistors. C251>C259 are DNI.
How and why are these to be installed, and how are the values determined? Some of the caps are designated as 3.3pF, but not all. I do not see any reference to these values or selection process in the EVM User Guide.
~Leonard