Hi,
Which cpp script files are used for the adc08d1520rb? I could not find anything bearing the name of the ADC.
Regards,
Supratim
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Which cpp script files are used for the adc08d1520rb? I could not find anything bearing the name of the ADC.
Regards,
Supratim
Hi Supratim
Two different types of script files are used with Wavevision 5, ones with .cpp suffix as you mentioned, as well as ones with .xml suffix.
The ADC08D1520RB uses a .xml script file. The full name of the file you are looking for is:
"adc10d1000_xc4vlx25_adc08d1520rb.reg.xml"
You should be able to find it in the following folder location:
C:\Program Files (x86)\National Semiconductor\WaveVision5\hardware\scripts
Best regards,
Jim B