Hello,
I have problem in CDCE62005 configuration -
1. Reading CDCE62005 manual I came to know that There are three options to select the input clock 1. PRI_REF 2. SEC_REF 3. AUX IN
2. But in DAC34SH84 GUI in CDCE input settings following are the options:
1. X
2. Manual_PRI_IN
3. Manual_SEC_IN
4. Manual_AUX_IN
3. Do I have to give external input to the DAC board ? or I can get some fixed frequency input to cdce by selecting given options?
4. How to make VCO range in 1.750 GHz to 2.356 GHz.