Hi, all
I would like to use high speed ADC, which is ADS5463. Its sampling rate is 500MPSP.
May I know is there any workable example with Altera platform?
Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Our TSW1400 capture card works with the ADS5463 EVM and that capture card uses an Altera Stratix FPGA. I have put in a request to get that code. Someone has to get that code ready for me for that particular EVM because the original author of the code made one Quartus project that had variables set in the Verilog to describe the format of the interface, so if i just grab the latest project it could be code set up for some other ADC instead of ADS5463. Whatever the last time the code was used is the ADC that it is set up for. I will let you know when itis ready.
Regards,
Richard P.
Hi,
I received a qar file as the quartus project for the ADS5463 to Stratix interface on the TSW1400. Please provide an email address and I can send it to you.
Regards,
Richard P.
Hi,
We do not have example code for the many different development platforms that are out there.
We do have the ADS5463 EVM working with the TSW1400 Capture Card, which does use an Altera FPGA. A Stratix IV I believe. The source code for the TSW1400 could be made available upon request, but considering the TSW1400 has to support many EVM formats the code for the ADC interface would not be as simple and readable as it could be if it were developed for a single data format. And it looks like that development platform you call out is Cyclone, not Stratix.
Regards,
Richard P.