Hi,
I have a simple question regarding WaveVision's ENOB calculation or better:
Is the ENOB increasing with increased Vpp or decreasing ?
We have the ADC16DV160HFEB eval board and we are playing around with different clocking strategies. For that we measure the ENOBs at different Vpp values of the input signal for a given clocking circuit.
We see the following ENOB(Vpp) curve (BLUE) when applying different Vpp values for given clocking circuit.
The IEEE spec says [1] (equation 71) that the ENOBs depend on Vpp and the amount looks right (see ORANGE curve, which is the relevant part of equation 71). But the spec also says, that the value is reduced by the amount, so we would expect a curve like the YELLOW one, approaching the highest ENOBs (~12.5) for maximal Vpp (2V or 2.4V).
If we now modify the „squared“ oscillator clock source to a more sinusoid waveform, the theory says, that we get less ENOBs. WaveVision 5 shows instead, that the ENOBs increase for a given Vpp.
So my assumption is, that WaveVison does a false ENOB calculation (I know I shouldn't do this). This results into the fact, that the customer is optimizing in the wrong direction and against the theory and mathematics ;-)
There is also a paper [2] from Walt Kester, who might now be working for TI, which says that the ENOBs increase with increasing Vpp (although he has a typo in the relevant section of equation 2). This is not what we see in WaveVision.
Can you shine some light into this ?
Looking forward to you answer,
Best Regards, Florian
PPS: I had posted a question a few days ago about the general dependency of ENOB and Vpp. I started a new post now about this - what I think – more Wavevision related problem.
[1] IEEE Standard for Terminology and Test Methods for Analog-to-Digital Converters, IEEE Standard 1241-2010
[2] http://www.analog.com/media/en/training-seminars/tutorials/MT-003.pdf