Hi,
I am working on a demo design with DAC37J82 EVM connected to a board with Lattice ECP5 FPGA through FMC connector.
I would like to use FPGA to configure the DAC37J82 and LMK04828 over the SPI interface via FMC connector.
I shorted 1-2 of the JP3, and I see that SPI signals are passing through the FMC to the CPLD but I am not sure if anything is written to the registers since all I get on SPI readout are zeros from both the DAC and LMK. I am trying to configure them in 4-wire SPI mode.
I am driving the FMC_SCLK, FMC_SDO, FMC_SEN_DAC, FMC_SEN_LMK signals, but I've noticed that the FMC_DIR_CONTROL also toggles when using SPI over USB. What are the requirements for this signal? What about FMC_B5 and FMC_B6 signals?
Is it maybe possible to get the CPLD design source code?
Thank you and regards,
Ana