Hello,
I am using DAC3484 EVM with xilinx VC707 board. Data is coming to DAC at 200 MHz data clock. With interpolation 1x, dac clock is also 200 MHz which is coming from on board PLL. The problem is that fifo collision alarm is going high.
I am using sync signal for both fifo read and write pointer reset. Sync signal is a periodic signal. It is 1 for 15 cycles and zero for 16th data clk cycle and then again 1 from 17th cycle to 31.
Is this correct sequence for sync signal? or should I do like :
sync signal is periodic signal with sync = 1 for 1 data clock cycle and zero for 15 data clock cycles and so on?
Following are register values