Hi,
I am using ADC16V130 in my design and as per ADC grounding discussion i have one solid ground plane for the my card.I am operating at about 42MHz and input signal is of 70MHz.Best ENOB i could achieve is only 10.5 bits.ADC interfaces to a FPGA sitting on other card through FMC connector.My colleges in my company say that because card has single ground and it is directly connected to noisy digital card through connector so noise floor of the ADC card is same as of digital card.Now i am planning for Re-CAD of the card with separate analog and digital ground planes and connecting DRGND pin to DGND.Will it help?? and if yes then will it be required to short AGND and DGND.