Hello
Due to the huge set of registers, we are having a hard time with determining the correct register settings.
First of all, we want to use the following mode as listed in Table 10 (DAC39J82 speed limits):
L = 8
M = 2
F = 1
S = 2
HD = 1
INTERPOLATION = 2
MIN FSERDES = 0.78125 Gbps
MAX FSERDES = 7 Gbps
MIN FDATA = 156.25 MSPS
MAX FDATA = 1400 MSPS
MIN FDAC = 312.5 MSPS
MAX FDAC = 2800 MSPS
MAX BW = 1120 MHZ
Based on these parameters, we need the input data rate, fDATA (or equivalently DACCLKP/N) which is seen on the left side of Figure 56 to be below to be 1320MHz and we need the DACCLK which is illustrated on the right of Figure 56 to be below to be 2640MHz. Here we need fSERDES to be 6.6Gbps. According to the formula on page 129 of the dac39j82 datasheet, for dual DAC, 8 lanes mode, the Serialized Data Rate per lane = fDATA*16*(10/8)*2/8 = 6.6Gbps).
Secondly, as mentioned in Table 10, we plan to use 2x interpolation and need the output sample rate fDAC to be 2640MHz. Also we need to use the Full Complex Mixer to shift the spectrum to the left by, for example, 1/4 of the fDAC.
Based on these characteristics, how do we configure the DAC38J82. Please assist.
Thank you.