If one wanted to clock the ADC08D1520QML-SP for a low sample rate of 250 MSPS, would that necessarily drop the power down from the typical 2W as specified on the data sheet?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If one wanted to clock the ADC08D1520QML-SP for a low sample rate of 250 MSPS, would that necessarily drop the power down from the typical 2W as specified on the data sheet?
Hi Peter
Power Consumption versus Sample Rate is shown in Figure 16 on page 24 of the ADC08D1520QML-SP datasheet. At 250 MHz clock rate the typical power consumption is around 1.4W.
Best regards,
Jim B
Jim,
Thank you again for the information. Another question I had, and just to confirm as this has come up before, is it possible to toggle the ADC ON and OFF (put in sleep mode) to save power? From the specification sheet, the calibration time for a 250 MHz input clock (and our sample rate) is about 6.4 ms.
Thanks,
Peter
Hi Peter
(Note: I'm the expert on the commercial version of the ADC08D1520. The space version expert may have additional comments regarding PD and Calibration issues specific to that version that I'm not aware of).
You can use the PD function to power-down the ADC and reduce power consumption.
However, if the device is powered down for a long time, the die temperature will drop from the previous steady state temperature where the calibration was done. When first powered up, the device performance (linearity, SNR, SFDR) will be reduced until the die temperature returns to a similar steady state temperature. Therefore, in this situation, if optimum performance is needed soon after power-up it would be best to perform a calibration at that time and then do another calibration when the device temperature stabilizes.
Best regards,
Jim B