Hello,
I am using DAC38J84 and few questions came up:
1. I am setting up NCO @ 100MHZ setting max gain reg 0x0C = 7FF , ( I am reffering to channel A) QMC is enabled output of the DAC terminated to 50R to GND and transformer. When I connect scope I see my signal around 100mV pk-pk @ 100MHZ. But according to the data sheet typical output current is 20mA I would expect signal to be around 1V. If there are any settings what I should have a look or can you please provide some advise how to increase amplitude of the output signal?
2. My digital section is not ready yet to drive JESD of the DAC, does DAC38J84 has an ability to generate some kind of test signal which can be probe at the output? I can control NCO and that's pretty match what I can see at the DAC output. Please advise.
Thank you,