Hi,
I'm bringing up DAC39J82 device.
Since I've got PLLs locked, SERDES LOS is cleared, FIFO alarms are gone, I want to check the pattern test.
I want to start with the alternating 0/1 pattern(TESTPATT set to 001).
What exactly is the alternating 0/1 pattern?
Is it like 0x0000, 0xFFFF, 0x0000, 0xFFFF,... ?
or 0x0000, 0x0001, 0x0000, 0x0001,..
or 0xAAAA, 0x5555,....