On the product description page for DAC34SH84EVM under the features section it is listed as directly compatible with the Altera HSMC headers on the Altera development boards. However, when I look at the schematics for the DAC34SH84EVM board I see that many of the 3.3V and 12V pins in the Altera HSMC spec are connected directly to ground on the DAC34SH84EVM board. Also the first 4 pins of the connector are tied to +6VDC on the DAC34SH84EVM while they are listed as signals in the HSMC specification. Am I missing something, it does not seem that the boards are compatible as the product page describes?