Hi All,
We plan to use DAC3482 for generating various signals as accurate as possibly.
The signals set span relatively big voltage dynamic range. (we have signals with small amplitude and also signals with high amplitudes)
The voltage adjustment in DAC3482 as far as I understood is by the coarse_dac(3:0) which provides 4 bit resolution.
Of course we may adjust the DAC data but we want to be full (or clos eto full) data scale if possible.
Initially I was thinking to connect voltage output DAC to VEXTIO but it seems only 0.6V - 1.25V is supported.
We need higher range
So I am thinking of using external current sink 6 or 8 bit SPI DAC connected to BIASJ pin.
Probably this is something standard I am trying to do and you can point me to a document giving me information and ideas in this respect?
Thank you in advance
Dimitar Penev