I am attempting to replicate the setup in the application report SLAA545 to setup a repeater application using the TSW1400EVM along with the ADS4249 and DAC3482 evaluation boards. I previously downloaded the firmware project from this forum and now am trying to program the Stratix IV device on the TSW1400.
Is this accomplished with the JTAG port or is there a configuration option in the High Speed Data Converter Pro v4.00 software?.
If it is using the JTAG port an the USB blaster can you give me some information on how to configure the jumpers on sheet 21 of the schematics of the TSW1400EVM to use the JTAG port. Also if this is setup can you give me some information on how you setup the various registers on the DAC and ADC evaluation boards as well. It looks like it would be possible to setup the jumpers on the ADC board to configure it but I'm not sure what I need to do on the DAC board.
Thanks,
Larry