Hello,
I am designing an UWB radio receiver which has a high speed adc at the end. The signal from the receiver includes pulses with width of ~3ns and I need to convert that signal to binary code using a recognition algorithm so that every pulse indicates 1 and no pulse indicates 0. I am considering using a combination of ADC12J4000 + TSW14J56 and HSDC Pro GUI. I have no experience in working with ADCs so I have a few questions:
1. The problem is that by reading the user guides I understood that I cannot implement an recognition algorithm with the HSDC Pro? Or is there a way to do that by using some back channel communication from HSDC to some other program? The HSDC is just for monitoring and saving the converted signal(?) but my application requires doing the conversion to binary code continuosly.
2. Or can I use some other GUI than the HSDC Pro?
3. I also found some other data capture boards (xilinx kintex-7 family?) to replace the TSW14J56 (and therefore the HSDC Pro) with but I'm not sure if they are capable of functioning in an application as fast as this one.
I'm not a native english speaker so I'm sorry for the typos and possibly unclear questions :)
Best regards,
Ismo