HI all experts
I have struggled on the JESD204B project with KC705 & 37J82EVM board
Basically, the KC705 is connected through FMC connector with 37J82EVM board
The test was based on the modification of JESD204B sample code using Virtual IO
The modified VIO is used for loopback test between TX and RX.
It is also used for generation pattern through FMC connector (from TX to DAC EVM board)
When PRAT pattern was selected, it seems like the system is working correctly (not sure yet)
The reason why I though this system is kind of working is that the system (DAC EVM) released tx_sync into JESD204B (but as I said above, I am not sure releasing tx_sync is enough to make a decision whether this system is working or not.
Another result of test is that
I attached FIFO & memory with JESD 204B for data streaming
When the attached memory system was used, DAC EVM doesn’t release tx_sync
Does anyone knows how I can I fix the problem?
and how I can decide that this system is working correctly or not?
If someone can help me, I am willing to attach the capture shot
(I don’t have a PC now)
I appreciate any help or comment
Thank you