Hello everyone,
I'm designing a board with a DAC3174 dual-channel DAC and am currently a bit unsure about power sequencing requirements:
1. The abs max ratings state that the difference between CLKVDD18, DIGVDD18 and VDDA18 must not be more than 0.5V, so these should be connected together with at most some passive isolation circuitry, correct?
2. Are there sequencing requirements between VDDA18 and VDDA33? I.e. is it necessary to somehow link the two voltage regulators to make one rise after the other?
3. What about IOVDD? Is it safe to have IOVDD powered while the rest of the DAC is not?
Thank you. Best regards,
Philipp Burch