Hi
First of all sorry for my Engish , i'm not the native speaker, but here is my problem:
I've bought DAC 5689 EVM board for broadband signal generation (for example LFM with band width about 40 -60 Mhz)
I've plugged 1.8 & 3.3 V (according datasheet's requirments, with less than 1A limit set per line), additionally 1-vrms, 0-v offset sine-wave signal provided as VCXO (as also required according datasheet). USB cable is connected too and "example" configuration (folder \Texas Instruments\DAC5689\Configuration Files\example.txt) loaded onto board via USB connection with DAC 5689 EVM Control tool.
Since i don't have special pattern generator to generate input, i''ve been using single square signal on top input bus leg (DA15)
My measurment results:
CLK2 & CKL2C configured in a proper way (clock for clock distributor CDCM is correct)
TXENABLE is high level
RESETB is high level
1.8V & 3.3V are present (no 5V since i don't need RF out)
Jumper positions
jP1 - 2-3 (set to internal ref)
j1 (unpopulated)
jP2 2-3 (using external VCXO)
jP3 2-3 (using externla VCXOB)
JP4 2-3 (CLKOUT)
JP5 2-3 (LOCK)
D2 & D3 light's ok (REF level & VCXO level), D1 Lock never light for me so as D4 Lock for DAC
Board passed through several reset-set cycles (starting with SW1 reset, programming with DAC5689 control tool, measurments) with always the same result at the end.(no visible output on r46, r56, r58, r69 even noise level is absent).
Could you please suggest some routines to start with to check if board function in correct way?
Also if there are some obvious mistakes durring attempt to start the board please let me know, thx.