I am facing following problems while working with TSW1400, TSW30SH84 and TSW1266 EVM.
1) I have Connected SMA cable from SYNC4 J17 on the Master TSW1400 EVM to the EXT_TRIG_INPUT J11 Slave TSW1400 EVM. When I have selected "Trigger mode enable” in Master TSW1400 EVM. Also both "Trigger mode enable" and "Arm on next capture button press" is selected in Slave TSW 1400 EVM. Then it is showing “No Trigger Occurred” at Slave TSW 1400.
But External Trigger is occurring when I have not selected "Trigger mode enable” in Master TSW1400 EVM. Also both "Trigger mode enable" and "Arm on next capture button press" is selected in Slave TSW 1400 EVM.
Why trigger is occurring at Slave TSW 1400 when Trigger mode is not enabled in Master TSW1400 from SYNC4 J17 only? Also there is no trigger out from SYNC1 J14, SYNC2 J15 and SYNC3 J16 in this configuration.
Why there is no trigger out from any of the SYNC4 J17, SYNC1 J14, SYNC2 J15 and SYNC3 J16 when Trigger mode is enabled in Master TSW1400?
Is there any issue in hardware or software?
2) How to provide same external reference clock of 10 MHz to TSW30SH84 EVM and TSW1266 EVM? How to check whether both are locked with same external reference clock. Please provide the configuration needed in both TSW30SH84 EVM and TSW1266 EVM.