I'd like to inquire about the ADS5401's track and hold operation. I've read the ADS5401 data sheet (SLAS946A - APRIL 2013 - REVISED JANUARY 2014), and, from the diagram on p. 24, I see that the track and hold circuitry operates at the full sampling rate, Fs. I, however, can't find any specs on how long this circuit is open for to sample the input signal. I believe this is sometimes referred to as the sampling window size or the sampling aperture time. In addition to knowing this value, I also need to know whether it is dependent on the input clock's frequency or any other parameters.
Thank you in advance for your help to understand the track and hold operation.