Hello,
I have in hand one WaveVision 5 board and one LM98640CVAL board. I have two question:
- Do I need the AFE evaluation software in addition of the WaveVision software? If yes where I can download it?
- On my board, there is no additional memories on it. Is the version with the four SRAM already exist and tested? If yes, it is possible to update my board myself with the rigth components?
Thanks
Matthieu Baque