This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Interface between ADS58J89-EVM and Xilinx KCU105 Evaluation board

Hello,

We've got a customer who wants to know if the ADS58J89-EVM will connect to the Xilinx KCU105 through the FMC connector without issues. They are specifically concerned that the U3B TTL has a 3.3V supply and the LVDS IO are driven from 1.8V supplies.

Any idea if this is going to cause problems?

(edited Subject line to correct part number, was ADS58J98)