Hello all,
I've had my fair share of troubles with this DAC in the past, and have decided to give it another go. I am using a TSW1400 to read a memory file which is then synthesized by the DAC. However, it seems *some* signals are properly synthesized, while others are not, and I'm not sure why. Here is an example of this:
As you can see, with the second signal, my guard band is not being synthesized. I have the clock going to a counter (with no reset), and the memory is simply cycled through.I wonder why this is not being properly synthesized by the DAC, when the 'volcano' signal is? Everything else in the setup is exactly the same.