I've got a custom board with an quad channel ADS54J54. Captures from the data stream show spurious responses at frequencies and harmonics of the LMFC frequency. I can change the value of K and these spurs move a predictable value. What would cause this?
These spurs show up when the input to the ADC is terminated. If an input signal is applied the spur remain in the same location. The signal input into the system appears as expected and without any unexpected harmonics. This removes the possibility of misinterpreting the data format.
Thanks.