Dear Sirs,
I am using the LM98640 in pattern generator mode. As I will have to connect the LVDS outputs to the inputs of an FPGA (no chosen at the moment), I will need to simulate with Hyperlynx to check the signal integrity of the differential lines (200MHz expected a DDR clock).
If the model doesn't exist for the LM98640, which one could I use which would be similar ?
Many thanks in advance