hello
I have two TSW14J56 boards which Im currently controlling from two laptops to create a tx pattern + rx capture solution
1. laptop1 - TSW14J56 + DAC (TSW38J84)
2. laptop2 - TSW14J56 + ADC (ADC12J4000)
I just have a simple query - is it possible to control all four boards (TSW+DAC, TSW+ADC) from a single laptop? From what Ive seen, I am unable to start two stand-alone versions of the HDSC Pro GUI on a single laptop so I suspect this is not possible? (USB 3.0 ports access is not the issue, just running multiple instances of the GUI on one PC to control multiple TSW14J56?)
Another quick query is to do with controlling the RF target frequency of the TSW38J84 via the Automation DLL (I run a Matlab script to set the Tx). Is there a command to set the RF frequency of the board? I can set the DAC settings (DAC data rate etc...) but I can find a command in the "HSDCPro Automation DLL User Guide" to control the RF target frequency? Can this only be controlled manually via the TSW38J84 GUI itself?
Any info greatly appreciated.
Marc