Is the Overrange bit synchronous with the output data bits i.e. is it true when the ADC output is at full scale (1FFFh or 2000h in two's complement mode) ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is the Overrange bit synchronous with the output data bits i.e. is it true when the ADC output is at full scale (1FFFh or 2000h in two's complement mode) ?
David,
Overrange bit is not synchronous with the output data bits. It will occur before the data. Unfortunately we don’t specify the OVR latency. It will be true per the data sheet section 8.3.7.6 as shown below.
Regards,
Jim