Hello
I want to use the DAC3484 with the following configuration:
DAC_REF=960MHz
Data rate for DAC1,2=240MSPS
NCO1 = OFF
Data rate for DAC3,4=100MSPS
NCO2 FREQ= 260MHz
DAC1,2 Output: Complex IQ BW of 200MHz
DAC3,4 Output: Complex IQ BW of 340-380MHz (upconvert using NCO)
My question is:
1. Is this setup applicable?
2. What is the minimum DATACLK freq?
3. Is there a way to reduce the level of the Nyquist at the DAC1,2 output (960M - DAC_output_Freq) besides placing a low pass filter?
4. Does the FPGA MAX10 family from Altera able to drive the DAC in this setup?
Thanks