Hi,
This query is regarding passive termination for current source DAC. I have gone through the application note SLAA399 – November 2008 (Passive Terminations for Current Output DACs). I have planned to use 1:1 transformer as represented in Figure 4 of the application note.
Can I increase the output power by not mounting the 100ohm parallel termination resistors? As per the calculations, the Output power will be -2dBm if 100 ohm parallel termination is used, 0.46 dBm if no parallel termination is used and -3.98 dBm if 50 ohm parallel termination is used.
Will changing the termination resistors, impact in any other parameters other than output power?
Kindly advise.
Regards,
Suresh Surya.B.S