Hello,
I have an application requiring 2 signals with 1GHz bandwidth and I would like to know if I am interpreting Table 11 correctly. I am assuming that the complex BW specified requires 2 DACs so I would need 8 lanes and 4 DACs operating in High density mode for a max BW of 1250MHz (first line of the table).
Would I be able to use the complex mixer to adjust the center frequency of both signals to 1.5GHz or would I need to perform such a task external to the chip?
thank you