This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC5688 Max Current of DVDD

Other Parts Discussed in Thread: DAC5688

Hi,

Could you tell me the DAC5688 maximum current of each pin for 1.8V?
I'd like to confirm the current of each mode (mode1-mode4).

1pin : CLKVDD  ?mA
10pin : DVDD1  ?mA
39pin : DVDD2  ?mA
44pin : VFUSE  ?mA
50pin : DVDD3  ?mA
63pin : DVDD4  ?mA


Regards,
itabi