Hello,
My customer have a question about DAC3482.
[Q]
Which of the following correct ?
(A) If they choose single sync source mode using SYNCP/N, then the value of syncsel_fifoin(3:0) and syncsel_fifoout(3:0) is "0001".
(B) If they choose single sync source mode using SYNCP/N, then the value of syncsel_fifoin(3:0) and syncsel_fifoout(3:0) is "0010".
(A) is written in datasheet P.78 config32 Function.
(B) is written in slaa584 P.8 Fugure 6.
Best Regards,
Hiroshi Katsunaga